Cancel
Showing results for 
Search instead for 
Did you mean: 

howto change operation subtype icons

Valued Contributor
Valued Contributor

How can you change the icons of the operation subtypes? I can't find it in the documentation. I can't find the icons either in the NX install folder. Are these icons perhaps included in the template file itself?

 

template operation subtype icons.PNG

W10 NX12.0.2.9
testing v1847
4 REPLIES

Re: howto change operation subtype icons

Legend
Legend

You can found the information on operation subtype icon customization in NX documentation, here:

CAM -> Manufacturing General -> Cam Customization -> Create a Template

 

CAM_ICON.JPG

 

NX icons files are not available since icons are embedded, however you can use bitmap files as explained in the documentation.

ciao

Re: howto change operation subtype icons

Valued Contributor
Valued Contributor

Aha! I mistook CAM_ICON for CAM_PICTURE. So, one problem solved, I can change the picture.

 

Is there a way to get a list of the mebedded icons?

W10 NX12.0.2.9
testing v1847

Re: howto change operation subtype icons

Legend
Legend

that's a little tricky, you have to set an environment variable:

 

PRINT_DIALOG_BITMAP_NAMES=1

 

and then you will find bitmap names in the syslog, for example:

 

...

&MACRO MENU, 0, UG_CAM_INSERT_OPERATION UG_GATEWAY_MAIN_MENUBAR <rbn_manufacturing_home.rtb->rbn_manufacturing_insert.grb> ## !
Used Dialog <Create Operation> Bitmap: floor_wall : SQ : LC
Used Dialog <Create Operation> Bitmap: floor_wall_ipw : SQ : LC
Used Dialog <Create Operation> Bitmap: face_milling : SQ : LC
Used Dialog <Create Operation> Bitmap: face_milling_manual : SQ : LC
Used Dialog <Create Operation> Bitmap: planar_mill : SQ : LC
Used Dialog <Create Operation> Bitmap: planar_profile : SQ : LC
Used Dialog <Create Operation> Bitmap: cleanup_corners : SQ : LC
Used Dialog <Create Operation> Bitmap: finish_walls : SQ : LC
Used Dialog <Create Operation> Bitmap: finish_floor : SQ : LC
Used Dialog <Create Operation> Bitmap: t_cutter_slot : SQ : LC
Used Dialog <Create Operation> Bitmap: hole_milling : SQ : LC
Used Dialog <Create Operation> Bitmap: thread_milling : SQ : LC
Used Dialog <Create Operation> Bitmap: planar_text : SQ : LC
Used Dialog <Create Operation> Bitmap: mill_control : SQ : LC
Used Dialog <Create Operation> Bitmap: mill_user : SQ : LC
&MACRO DIALOG_BEGIN "Create Operation" 0 ! DA1

Re: howto change operation subtype icons

Valued Contributor
Valued Contributor

Works great, thanks!

W10 NX12.0.2.9
testing v1847

Learn online





Solution Information