Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

load tbcload.dll file output

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
# ***************    a.tcl  **************************
# TclPro::Compiler::Include # ########### OUTPUT "12345" ################# ## proc PB_CMD_1 { } { ## MOM_output_text "12345" ## } ########################################### set dir [MOM_ask_env_var UGII_CAM_POST_DIR] package ifneeded tbcload 1.3 [list load [\ file join $dir tbcload13.dll]] if {[catch {package require tbcload 1.3} err] == 1} { error "The TclPro ByteCode Loader is not available or does not support the correct version" } tbcload::bceval { TclPro ByteCode 1 0 1.3 8.3 1 0 11 5 0 0 4 0 4 1 1 -1 -1 11 (<E<!(H&s!+-!! 1 z 1 +! 5 x 4 ,CHr@ x 9 V/NX6^1CO9%v x 1 A! p 1 0 7 2 0 0 4 0 2 1 1 -1 -1 7 w0E<!)'!! 1 z 1 '! 2 x 15 j<OV?@5--E4-0CFsHE- i 12345 0 0 0 0 x 15 rpwhC;Z2b3<?<+EfqT+ 0 0 }

###source file  test.tcl code:

source "${cam_post_dir}a.tcl"

 

test_output_PB1.JPG

test_output_PB2.JPG

error:

test_output_err.JPG

 

Please help me !!! Thank you very much!

35 REPLIES 35

Re: load tbcload.dll file output

Phenom
Phenom

I am not sure what you are asking. You are trying to use tbc encrypted files? Or you are saying that you are just trying to source a tcl? Where did the tclpro dll code come from? Look at an example from Janus (if you are trying to do this intentionally.) They encrypt with tclpro in a couple examples I have seen in the past (but don't have.) 

NX12.02
Windows 10 Pro
ITC Inc.

Re: load tbcload.dll file output

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

You are trying to use tbc encrypted files?   YES

 

 tclpro1.41 encrypted !!!

 

use tbcload13.dll file decrypt ,but the results of error.

 

 

 Only support TCL8.3 ?

Re: load tbcload.dll file output

Phenom
Phenom

You probably need to use the 1.4 dll. There is a tbcload14.dll.

NX12.02
Windows 10 Pro
ITC Inc.

Re: load tbcload.dll file output

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Very happy to see your reply, thank you!!

 

But didn't you said this file

32111.JPG

Re: load tbcload.dll file output

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Error in NXpost.But There is no problem in wish83.exe!

Please help me to test it? Thank you!!!

--------------------------------------

Tclpro:

http://www.tcl.tk/software/tclpro//eval/1.4.html

--------------------------------------

 

888.JPG

Re: load tbcload.dll file output

Phenom
Phenom

I can't really help with the tclpro only used to encrypt a little code. I have used the tbc and the dll's. I installed TCLPro 1.4 at some point and the dll was there - so I pulled it out of there. Do a search for a tclpro version that includes the dll - install it - and get the dll out of it. The compile exe in version 1.3 still works for both.

NX12.02
Windows 10 Pro
ITC Inc.

Re: load tbcload.dll file output

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

thanks!

You used NX8.5 version ?

Re: load tbcload.dll file output

Phenom
Phenom

Yes. 1.4 was necessary with NX8.5 I think.

NX12.02
Windows 10 Pro
ITC Inc.

Re: load tbcload.dll file output

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Why do I always test was not successful!!!

 

The tbcload14.dll directory in ...\MACH\resource\postprocessor ?

 

tbcload1.4:

http://www.darvision.com/ftp/Daejeon/HD_DVM_DATA/DVM62_Burn_080727/tcl/lib/tbcload1.4/

 

 

Learn online





Solution Information