Cancel
Showing results for 
Search instead for 
Did you mean: 

location for cdl files

Pioneer
Pioneer

in Postbuilder - in the "include other cdl file" option

 

does the cdl file have to be in the "$UGII_CAM_USER_DEF_EVENT_DIR/"

has anyone tried to put it somewhere else.  Like in the postprocessor dir in the installed machine folders?

It seams like I can paste this in the msg box

$UGII_CAM_LIBRARY_INSTALLED_MACHINES_DIR/TR_electrodes/postprocessor/haas/TR_UDE.cdl

but how does NX know to use this cdl file.  Does it look in the post when you select the machine from the library?

 

3 REPLIES

Re: location for cdl files

Phenom
Phenom

You can put the cdl in the post directory - I do. I just name it something other than the cdl (potentially) created by postbuilder (I assume you are talking about a manually created one.) The def file at the top has the cdl post paths.

NX12.02
Windows 10 Pro

Re: location for cdl files

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

If you move the .cdl file to another folder you will need to modify the line in the configuration file that "points" to the location

for example

USER_DEFINED_EVENTS,H:\UG\NC\UDE\test.cdl,${UGII_CAM_USER_DEF_EVENT_DIR}ude.tcl

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race
Highlighted

Re: location for cdl files

Phenom
Phenom

We run customized ude lists (cdl) that load with the machine. If no machine is loaded - the cdl in the user_def_events directory is used. We don't modify configuration to have a cdl determining the machine specific udes available. The library installed machines dir variable points to the post area.

NX12.02
Windows 10 Pro

Learn online





Solution Information