Cancel
Showing results for 
Search instead for 
Did you mean: 

machine code simulation error

Valued Contributor
Valued Contributor

I am trying to get my first simulation going. When I choose to tool path simulate it is running ok. When I go to machine code simulation I get the pictured error, why? I also notice if I have twin turrets that all the movements are being done with the main turret. If I need to use the main spindle as a C axis, it doesn't rotoate. I notice the simulation examples from siemen do this too.

 

error.jpg

Using NX 8.0.3.4
3 REPLIES 3

Re: machine code simulation error

I think we'll need more details to determine the cause.

Have you gone through this with GTAC?

Mark Rief
Retired Siemens

Re: machine code simulation error

Valued Contributor
Valued Contributor

I was hoping there would be a quick solution before getting all the documents to GTAC. There is just so much data everywhere for machine simulation that I understand your reply.

Using NX 8.0.3.4

Re: machine code simulation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The error message is not telling anything useful, at least a syslog would be needed.

An image of the machine tool builder navigator with all columns enabled and visible would be helpful too.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information