Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

machine simulation

Pioneer
Pioneer
colisão maquina1.jpg 
the simulation machine has even crash the tool being not touching the piece
the machine I'm using and the Mikron UCP 800

1 REPLY 1

Re: machine simulation

What are the clearances set to in the operation? 

For example, if the holder clearance is 3 mm, a collision will be reported if the distance between the holder and part is less than 3 mm.

Mark Rief
Retired Siemens

Learn online





Solution Information