Cancel
Showing results for 
Search instead for 
Did you mean: 

machine tool builder <turning machine>

Creator
Creator

hai....

i need a demo video for machine tool builder "turning machine". 

if any one having, please sent avideo link or any other source file

6 REPLIES

Re: machine tool builder <turning machine>

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

there is no video available which explains the Machine Tool Builder application in conjunction with a turning machine. But there are several out of the box examples which can be reused. I hope one of them fits to your needs.

 

2019-02-07 08_59_26-NX - Manufacturing.png

 

These kits are located under: 

...\MACH\resource\library\machine\installed_machines\

 

and the nc simulation samples under:

...\MACH\samples\nc_simulation_samples\

 

Thomas

Re: machine tool builder <turning machine>

Creator
Creator

@thomasfeind 

thanks for reply

but its not help for me. because i already refer that example.

there is problem in tool place in turret (angle of tool) and machine code simulation error

Re: machine tool builder <turning machine>

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

please add a screenshot from your channel configuration and the machine node in Program Manager. It seems that the channel name does not match the name ('Main') in the machine ini file.

Thomas

Re: machine tool builder <turning machine>

Creator
Creator

thanks @thomasfeind 

i find and slove that problem. that not my major problem. my problem is tool mounting.

i was check and correct my axis and coordinate. but it not fix corect position. please show how to slovw it 

 

 

 

 

thanks you,

 

Re: machine tool builder <turning machine>

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

for parameter turning tool the defined turning plane defined the initial orientation.

Additional the turret angle define inside the  KIM of the pockets takes into account to bring the tool into orientation. To move it out there are  X/Y values on the More tab.

Hope that helps

 

pocket rotation angle.png

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: machine tool builder <turning machine>

Creator
Creator

HI  @SpaceTom 

  THANKS FOR THE REPLY . I WILL TRY AS YOU SAID 

 

 

 

 

THANKS @Gogo 

Learn online





Solution Information