Cancel
Showing results for 
Search instead for 
Did you mean: 

mill turn PP, drilling in radial direction

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

I create mill-turn PP, but I have problem when I drill in radial direction.
The output is not OK, it´s drill in axial direction.

1.PNG2.PNG3.PNG
Whan I need to put in my G code, that output will be OK (G68.2/G68.5).
The controller is mazak smooth C.
Can somebody fix my G code (attachment)?

 

 

8 REPLIES 8

Re: mill turn PP, drilling in radial direction

Gears Phenom Gears Phenom
Gears Phenom

How do you know that it is drilling in axial direction?

To be honest It looks OK to me.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: mill turn PP, drilling in radial direction

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is this a control that wants to use G83/84/85 for "axial" and (?) G86/87/88 (or is it 87/88/89?) for radial?

Is that the issue?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: mill turn PP, drilling in radial direction

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi,

It´s need to be G68.5 and somethings (I,J,K controller is mazatrol).

Re: mill turn PP, drilling in radial direction

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

It´s not ok. It´s need to be radial direction.

 

Look MCS. The hole is in Y direction, not in Z direction. It´s for mill turn machine.

123.PNG

Re: mill turn PP, drilling in radial direction

Gears Phenom Gears Phenom
Gears Phenom

Dont understand.

MCS is ok. Hole is in radial drection. And you have output what looks good.

If it is mill turn like lathe with turret with live tools. Dont see reason for some G68...

Tool axis is X or Y, plane G18 or G19.  

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: mill turn PP, drilling in radial direction

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

we put this G code on the machine and it´s not OK.

Drilling is in axial direction.

Re: mill turn PP, drilling in radial direction

Phenom
Phenom

Assuming tooltip comp is handled ok somehow (don't see G43.x) and if G18 not working in example you have - below would be straight G68 example as I see it:

N9 G54

N10 G98 G97

N11 (G18)

N12 M200

N13 M203 S2450 M8

G68 X0 Y0 Z0 I0 J1 K0 R90

N14 G0 X25.000 Y0.000 Z110.000 C90.000 M211

N15 G83 X25.000 Y0.0 Z35.000 R96. F1850.

N16 G80

NX12.02
Windows 10 Pro

Re: mill turn PP, drilling in radial direction

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hi,

Thanks a lot.

Best regards.
Edin

Learn online





Solution Information