Cancel
Showing results for 
Search instead for 
Did you mean: 

mill/turn

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

When milling the face of a part on lathe. where is the milling mcs csyc located at?  use same a lathe or is mcz parallel with lathe z likea  typical m-c machine? 

2 REPLIES 2

Re: mill/turn

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Machines I've seen, I can use the same MCS for the milling & turning  MCS Z is the same way for both.(along turning spindle centerline)

Note it has  to be an MCS created from the "turning" part template (not from a milling template file)

If you want some of the "milling only" stuff (avoidance, clearance, etc.) create a subsidiary one that is that stuff only.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: mill/turn

I would look at this sample:

Help > Manufacturing Tutorials > Open a sample part > cam_sample_mill_turn

 

To create a new setup, look at:

File New > Manufacturing > Mill Turn Express

 

Mark Rief
Retired Siemens

Learn online





Solution Information