Cancel
Showing results for 
Search instead for 
Did you mean: 

nx cam received an error 1740001

Experimenter
Experimenter

Hello friends
when post-processing operation, the program reports an error 1740001

Безымянный.jpg

 

i need help. please

 

5 REPLIES 5

Re: nx cam received an error 1740001

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NX CAM is looking for the indicated file, and it cannot find it.

If you don't know where the ENV variable UGII_CAM_LiBRARY_INSTALLED_MACHINE_DIR is pointing to, look in the syslog.  The exact menu picks vary by version, but it is something like:

Menu -> Help -> Log File

In the "Information" window, search for that ENV variable

 

You will have  to figure out how to fix it from there

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: nx cam received an error 1740001

Experimenter
Experimenter

please tell me how to do this in detail.

 

nx 10.0.0.24

os win 7 X64

Re: nx cam received an error 1740001

In your NX session, go to Menu > Help > Log File.

Search for UGII_CAM_LIBRARY_INSTALLED_MACHINES_DIR and see where it is pointing. For example:

UGII_CAM_LIBRARY_INSTALLED_MACHINES_DIR d:\users\rief\nx11\resource\library\machine\installed_machines\

In a file explorer window, browse to this location, then navigate through the folders shown in the error message, and see it the file exists. 

If you still can't figure it out from this, please contact GTAC and they can help you diagnose this.

 

 

Mark Rief
Retired Siemens

Re: nx cam received an error 1740001

Experimenter
Experimenter

hi Mark

I have made as you have told
I have established in the file in the folder H:\Siemens\NX\10.0\MACH\resource\library\machine\installed_machines

 

also I have received this error message

26081040.png

 

 

 

 there is a log file

Re: nx cam received an error 1740001

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

When you see the "Error in do_event" message you have to look in the syslog to find the tcl error.

Open the syslog (thanks for attaching it!), scroll to the bottom, then scroll up to the top of the "crash dump", for the "***TCL_ERROR***" line

In your case, this is

***TCL_ERROR***: Event Handler: H:\Siemens\NX 10.0\MACH\resource\library\machine\installed_machines\CTXGamma1250TC_V10_CS_TS\postprocessor\CTXGamma2000TC_HA_mm.tcl, Event: MOM_start_of_path, Error: can't read "rg_param(717)": no such element in array
    while executing
"MOM_output_literal " RG717=$rg_param(717)         ;CLAMPING DEPTH""

 

So in the "start of path" event, you are calling (a few lies after the above) PB_CMD_output_program_head, which eventually tries to output the above line, and the variable rg_param(717) doesn't exist.

 

I'm not sure where you define that variable (if ever) but you will have to track down why it isn't defined.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information