Cancel
Showing results for 
Search instead for 
Did you mean: 

okuma lathe post

Experimenter
Experimenter

Hi all,

I want the post to ouput the workpiece limits as a block like that

 

PS LC,[ 320 ,0],[ 320 , 150 ],4

 

it is for okuma lathe, how can i do that?

 

Any one has an okuma lathe post?

 

Many thanks

2 REPLIES

Re: okuma lathe post

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For my turning/mill-turn machines, I typically have a seed part that contains a sketch defining the blank.

I can then extract the sketch expressions (using MOM_ask_ess_exp_value) to get the data for commands like this (or for Siemens controls, the WORKPIECE command).

 

Another option is a UDE, but then the data is not associative to the geometry used for the turning blanks.

 

Note expression and attribute data is available in "start of program" event. 

Note UDE data is NOT available in "start of program", (and not even in "start of path") so you may have to play a bit with when things are output to get the PS commands in the correct place.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: okuma lathe post

Gears Phenom Gears Phenom
Gears Phenom

There are several Okuma posts in the PB library

 

Help - Online Technical Support - Download NC Post Processor

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information