Cancel
Showing results for 
Search instead for 
Did you mean: 

part geometry

Pioneer
Pioneer

Hello, Guys

 

I use 5 axis mill operation (veriable contour).Then I select workpiece as part geometry. When I generated. Tool path is confused. then change to MCS as part geometry. It is ok. Why?

 

Thanks!

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
2 REPLIES

Re: part geometry

Esteemed Contributor
Esteemed Contributor

Can you provide a sample part file, since there are too many drive methods you can use to solve this from the top of ones head.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk Testing: NX12.0 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink

How to Get the Most from Your Signature in the Community

Re: part geometry

Many of the drive methods in surface contouring do not require PART geometry. With PART, the drive path is project to the PART, but without PART, the drive path is used without projection.

My guess is that when you change the geometry parent to MCS, there is no PART geometry, so you are seeing a non-preojected path. 

Mark Rief
Retired Siemens

Learn online





Solution Information