Cancel
Showing results for 
Search instead for 
Did you mean: 

point to point drilling - no cycle

Pioneer
Pioneer

Anyone know if it's possible to drill point to pont using no cycles?

 

Kind of like teach mode, but teach mode is only in turning?

 

Like to keep it simple.

 

thanks for any input.

 

Cyl

 

 

7 REPLIES 7

Re: point to point drilling - no cycle

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you have the licenses, "generic motion" operations are the equivalent of the turning "teach mode".  Otherwise you can set the cycle to "Standard text" or "no cycle"

If you are trying to do something at each point (e.g. some special cycle), if you use "Standard text", then add a UDE to the operation, then over-ride proc MOM_drill_text_move to output whatever you want.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: point to point drilling - no cycle

Pioneer
Pioneer

How do I find 'generic motion' if I have the license?

 

Under 'create operation' -> type?

Re: point to point drilling - no cycle

Phenom
Phenom

mill_multi_axis - hand with a little 2 next to it (icon.)

NX12.02
Windows 10 Pro
ITC Inc.

Re: point to point drilling - no cycle

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

What kind of output are you looking for?

 

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: point to point drilling - no cycle

Pioneer
Pioneer

This is on a Olympia HBM. It has a B-Axis Rotary around Y-axis. The controller is Siemens 840D.

Replace Cycle82 with normal G0 and G1 along the tool axis - Z-axis.

Current code:

 

N8665 Z1000.
N8670 Y46.7 Z1121.587
N8675 F500.
N8680 MCALL CYCLE82(1081.5872,1075.5872,6.,1073.8172,,1.)
N8685 X0.0 Y46.7
N8690 MCALL
N8695 G0 Z1000.

 

The post needs work to keep X at zero and rotate B only, otherwise I could use multi-axis -> generic motion. Just trying to find something quick to work now. Someone said I can change the cycle to linear and post will output regular G code?

Re: point to point drilling - no cycle

Pioneer
Pioneer

Hello.

 

I made it work using NO CYCLE and adding GOTO Points before and after in Start and End Events.

 

Thanks

Re: point to point drilling - no cycle


@cyl wrote:

Anyone know if it's possible to drill point to pont using no cycles?

 

Kind of like teach mode, but teach mode is only in turning?

 

Like to keep it simple.

 

thanks for any input.

 

Cyl

 

 


In the old point to point operations, you can set the Cycle type to No Cycle - the result is a point to point milling path.

But as said before - Generic Motion is the way to do this now. It is the "teach mode" of milling. 

Mark Rief
Retired Siemens

Learn online





Solution Information