Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

post edit

Creator
Creator

Good morning everyone,

I was wondering if someone could help me with a post issue for heidenhain conversational.I need to have  a L on the rapid lines example are lines 7,8,9

 

any help appreciatedSmiley Happy

 

0 BEGIN PGM 100 INCH
0001 ; POSTPROCESSOR NAME
0002 ; C:\USERS\MSTAPLETON\DESKTOP\MIKES POST\MIKE_CONVERSATIONAL.TCL
0003 BLK FORM 0.1 Z X0.0 Y0.0 Z-20.
0004 BLK FORM 0.2 X100. Y100. Z0.0
0005 TOOL CALL 4 Z S1000
0006 L Z4.088 W0.0 F MAX
0007 L X9.862 Y-3.2469 FMAX M3
0008 Z4.0879
0009 Z3.9707
0010 L Z3.8707 F100. M8
0011 L Y-3.3469
0012 L Y-10.3932
0013 L Y-10.4932
0014 L Z3.9707
0015 Z4.0879
0016 X8.5773 Y-3.2469
0017 Z3.9707
0018 L Z3.8707
0019 L Y-3.3469
0020 L Y-10.3932
0021 L Y-10.4932
0022 L Z3.9707
0023 Z4.0879
0024 X7.2925 Y-3.2469

2 REPLIES 2

Re: post edit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Assuming the "L" is required on EVERY "rapid" move line

a couple options

1) Add as text to appropriate line(s) in rapid move event, make sure it is "forced" and /or make it non-modal

 

2) Add a new Word "L_rapid".make sure it is marked non-modal

add to rapid move blocks

You may still have to force it.

 

If my assumption is not correct, let me know what the issue really is.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: post edit

Creator
Creator

Thank you Ken_A

Option #1 worked gr8 Smiley Very Happy

Learn online





Solution Information