Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: post for probing 840D SL cycles

Gears Legend Gears Legend
Gears Legend
It would be sufficiënt if (siemens) NX would support the OOTB sinumerik cycles. For a start some basic cycles like point, hole/shaft, web/groove would be ni
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: post for probing 840D SL cycles

Siemens Pioneer Siemens Pioneer
Siemens Pioneer
Hello,

there are news about this topic?

I have same problem.
Anyone ave some solutions?

Thanks
Emilio

Re: post for probing 840D SL cycles

I believe probing_cycles_siemens and probing_cycles_fanuc posts are intended to be used with "Inherit UDE From A Post" so you can add probing cycles to an existing post.   

NX 12.0.2

Re: post for probing 840D SL cycles

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Sorry probably there are a misunderstood.

My question is reference to Sinumerik 840d probing cycle (CYCLE976, CYCLE977, CYCLE978, ecc.).

Anyone have implement that in a post?

Re: post for probing 840D SL cycles

Genius
Genius

So are 840D probing cycles available yet?  I am still only seeing Renishaw cycles in the probing_cycles_siemens.pui

Re: post for probing 840D SL cycles

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!

Yes, we have implemented ALL Siemens Sinumerik 840D sl measuring cycles in postprocessor AND inside template part probing.prt

Cycle997.pngHole or Boss Measuring

 

Cycle998.png

CYCLES.png

Highlighted

Re: post for probing 840D SL cycles

Genius
Genius

Hi Yuri!

 

That looks great.  What version of NX is that in?  And is it specific to Post Configurator?

Re: post for probing 840D SL cycles

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

NX9.......NX1847........NX1872.........................NX2020(I hope...)

 

No. Just PostBuilder

Learn online





Solution Information