Cancel
Showing results for 
Search instead for 
Did you mean: 

post for probing 840D SL cycles

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

In C:\Program Files\Siemens\NX 10.0\MACH\resource\postprocessor there is a postprocessor -probing_cycles_siemens-

This post was last updated in 2008. Using this with the ootb NX probing operations you don't get anything usefull for a modern sinumerik controller.

;Probe Hole 100 mm
N1161 G0 X0 Y0 Z400. D1
N1162 R24=0 R25=0 R26=297 R9=20000 R13=0.0
N1163 L9810
N1164 R24=0 R25=0 R26=310 R9=20000 R13=0.0
N1165 L9810
N1166 R7=15 R11=100 R18=0 R20=01 R21=.25
N1167 L9814
N1168 R24=0 R25=0 R26=400 R9=20000 R13=0
N1169 L9810

 

Why doesn't Siemens NX support it's own controller?

 

Does anyone have a post that supports the standard 840D SL measuring cycles?

 

;Probe Hole 100 mm
G0 X0 Y0 Z400
CYCLE977(1001,,,1,100,,,5,1,0,-21,20,,,1,"",,0,1.01,1.01,-1.01,,,,,1,1)
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET
17 REPLIES 17

Re: post for probing 840D SL cycles

Phenom
Phenom

I agree. The on machine probing forms are tailored more toward renishaw. I have a couple projects where I chose not to use it for siemens probing.

NX12.02
Windows 10 Pro

Re: post for probing 840D SL cycles

Pioneer
Pioneer

I also agree.  I was doing some searching around last week on this and was surprised that I couldn't even find anyone talking about this.

 

Re: post for probing 840D SL cycles

Phenom
Phenom

If you look at the output - it is renishaw cycles on a siemens control (which is available.) The siemens probing cycles are quite different - I think the forms would need an update - as well as (potentially) verify playback.

NX12.02
Windows 10 Pro

Re: post for probing 840D SL cycles

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I have vague (mis?) memories of Siemens saying that when they implemented on-machine probing they would start with Renishaw (presumably because it is the most widely used cross-platform solution).  IIRC they implied they may start supporting other solutions in the future.

 

I would suggest filing ERs so they know it is important to you to implement Siemens probing (although if they don't have it already, by the time they do have it you may have already done your own thing...)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: post for probing 840D SL cycles

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
You would expect that Siemens would support it's own cyles by now.
You could also expect that they check this community every now and then to see whats hot.
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: post for probing 840D SL cycles

Patrick,

We monitor this community quite intensely.

I have asked for details on our support of probing cycles. 

Mark Rief
Retired Siemens

Re: post for probing 840D SL cycles

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
I am aware and your input is being appreciated.
Today I filled a ER on this (trough our representative)
Lets hope development is already working on this
Patrick Delisse
KMWE - Aero Engine
NX 12.0, TC 11.2, CAMPOST V22, Vericut 8.2, TDM 4.8
C#, VB, .NET

Re: post for probing 840D SL cycles

Pioneer
Pioneer

Mark have you heard anything back on this yet?

 

Re: post for probing 840D SL cycles


@smoffat wrote:

Mark have you heard anything back on this yet?

 


Only that it's more complicated than I thought, and UDEs are required.

One complication is that the cycles are often altered from the OOTB Siemens cycles. 

 

Our management is aware of the situation, but I don't know the status.

Mark Rief
Retired Siemens

Learn online





Solution Information