Cancel
Showing results for 
Search instead for 
Did you mean: 

postprocessor for TRAK DPLM

Experimenter
Experimenter

Does anyone have a post written for a TRAK DPLM conversational mill?  We just bought 2 of these machines, so any help would be appreciated.

 

Thanks, Steve

6 REPLIES

Re: postprocessor for TRAK DPLM

Esteemed Contributor
Esteemed Contributor

There's one in  the on-line post library:

https://download.industrysoftware.automation.siemens.com/unigraphics/pb_posts/post_index.htm

 

No idea how good it is.

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: postprocessor for TRAK DPLM

Experimenter
Experimenter

It's not good - that's why I reached out on this site.  Thanks for the reply!

Re: postprocessor for TRAK DPLM

Phenom
Phenom

I am curious - what format of code does it need? All I see on the internet is how to do the conversational programming (at machine - screens - "events".) Do you have an offline generated code example? That post from the siemens site was just a template opened and saved in PB5 - nothing in it.

NX10.03
Windows 7 Pro

Re: postprocessor for TRAK DPLM

Experimenter
Experimenter

The machines take G-code, and I've found that the 3axis mill post within NX is close, with a couple edits needed.

Re: postprocessor for TRAK DPLM

Esteemed Contributor
Esteemed Contributor

Not sure about your machine, but one I have dealt with will take 2 formats.

 

- One with full 3 axis motion, but is missing a couple drill cycles (and I never got helical output to work)

 

- One with 2.5 axis motion (i.e. you can't have Z motion with either X or Y) - has more cycles, and the control will translate into their internal "GUI driven" program format

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: postprocessor for TRAK DPLM

Experimenter
Experimenter

Ken,

 

If you don't mind sharing them, I'm happy to give them a try.

 

Thanks,

 

Steve

Learn online





Solution Information