Cancel
Showing results for 
Search instead for 
Did you mean: 

probe dia output / tracking

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

anyone know why im getting an extra .100 added into my probing output?  i cant find any way to use a tracking point in the probe sub ops.  i have also tried the OOTB renishaw post.  it seems like the OOTB probe may be .200 dia and i just dont know how to use it or tracking points corectly

 

while pobing a wall @ Y6.00 i get posted output of  P9811 Y6.1 S54.  S/B P9811 Y6.0 S54

same with the x direction when probing a wall @x-2.00 i get P9811 X-2.1 S54 and it S/B P9811 X-2.0 S54

 

thanks, Damian

 

 

%
O0001
(PROGRAM FILE NAME: MODEL_TEST_PROBING_MFG.NC)
(PROGRAMMER damian.forsythe WED, FEB 04, 2015 07:10)
(MACHINE: HAAS VF 3 AXIS)
(POST NAME: Renishaw_Probe_3ax_2-2-15)
(NOTES: UNPROVEN PROGRAM)
(PROBING_X_Y)
N0025 G40 G17 G00 G90 G70
G91 G28 Z0.0
T25 M06 (HAAS PROBE)
G65 P9810 X0.0 Y6.35 Z3. F400.
G65 P9810 X0.0 Y6.35 Z1.4 F400.
P9811 Y6.1 S54
G65 P9810 X0.0 Y6.35 Z3. F400.
G65 P9810 X-2.6 Y5.6 Z3. F400.
G65 P9810 X-2.6 Y5.6 Z1.4 F400.
P9811 X-2.1 S54
G65 P9810 X-2.6 Y5.6 Z3. F400.
G28 Z0.0
M30
%
============================================================
Information listing created by :  damian.forsythe
Date                           :  2/4/2015 7:10:54 AM
Current work part              :  C:\IN WORK\PROGRAMS\Model_test_probing\MODEL_TEST_PROBING_MFG.prt
Node name                      :  cei-3269
============================================================
Information Units    Inches
Point                XC =    0.00000000000        X =    0.00000000000    
                     YC =    6.00000000000        Y =    6.00000000000    
                     ZC =    2.00000000000        Z =    2.00000000000    
 
------------------------------------------------------------
 
 
============================================================
Information listing created by :  damian.forsythe
Date                           :  2/4/2015 7:11:00 AM
Current work part              :  C:\IN WORK\PROGRAMS\Model_test_probing\MODEL_TEST_PROBING_MFG.prt
Node name                      :  cei-3269
============================================================
Information Units    Inches
Point                XC =   -2.00000000000        X =   -2.00000000000    
                     YC =    4.50000000000        Y =    4.50000000000    
                     ZC =    2.00000000000        Z =    2.00000000000    
 
------------------------------------------------------------
 
 
============================================================
Information listing created by :  damian.forsythe
Date                           :  2/4/2015 7:13:48 AM
Current work part              :  C:\IN WORK\PROGRAMS\Model_test_probing\MODEL_TEST_PROBING_MFG.prt
Node name                      :  cei-3269
============================================================
Information Units    Inches
Point                XC =   -8.65377948673        X =   -8.65377948673    
                     YC =    3.46217578138        Y =    3.46217578138    
                     ZC =    0.00000000000        Z =    0.00000000000    
 
------------------------------------------------------------

 

14 REPLIES 14

Re: probe dia output / tracking

I'm guessing you're saying that it's adding the radius to the Z output.  I had this problem and I ended up just putting geometery into the tool assembly so that it would track the bottom.  If I clicked on the ruby sphere it would track everything from the ceter of the ball.Capture.JPG

Jake Hardwick
CNC Programmer
Senior Aerospace AMT
Production NX8.5.3.3 Beta testing NX10.0.1.4

Re: probe dia output / tracking

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

 

z is working fine.  its X and Y direction that are showing to be off by .100.

 

to me it seems the probe is moving to the intended wall located at X6.00 and its using some sort of tracking point or offset that is keeping the c/l of the pobe off the wall by .100 resulting in a posted output of X6.1  i huess what im after is just c/l output of the probe.

 

when i change tool from probe to none,  i get the corect output of x-2.0 and y6.0 so it must have something to do with the probe and or lack of tracking points.

 

(PROBING_X_Y_COPY)

G65 P9810 X0.0 Y6.25 Z3. F400.

G65 P9810 X0.0 Y6.25 Z1.5 F400.

P9811 Y6. S54

G65 P9810 X0.0 Y6.25 Z3. F400.

G65 P9810 X-2.5 Y5.6 Z3. F400.

G65 P9810 X-2.5 Y5.6 Z1.5 F400.

P9811 X-2. S54

G65 P9810 X-2.5 Y5.6 Z3. F400.

G28 G00 G91 Z0.0

 

Re: probe dia output / tracking

Did you specify a tracking point when building the tool? Also, try adding the set tacking point sub-op.  You can use Ken's MOOG_Show_Globals to see if there is an array that contains the numbers you're looking for.

capture.png

Jake Hardwick
CNC Programmer
Senior Aerospace AMT
Production NX8.5.3.3 Beta testing NX10.0.1.4

Re: probe dia output / tracking

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Thanks Jake,

 

I think you nailed it with the tracking point sub op.  I cant figure out how to create a new probe model and save into a library or abb tracking points to it.  very different from standard tools and tracking points.  using the default probe it will not allow tracking points as shown in the pic.  no matter what i enter the OK button will not activate.

Re: probe dia output / tracking


@dforsythe wrote:

Thanks Jake,

 

I think you nailed it with the tracking point sub op.  I cant figure out how to create a new probe model and save into a library or abb tracking points to it.  very different from standard tools and tracking points.  using the default probe it will not allow tracking points as shown in the pic.  no matter what i enter the OK button will not activate.


If the OK button will not activate, something required is not specified.

 

In the help, search for the section "Add a solid tool to the tool library"

The basic process:

Open the part file with the probe model.
Create a new CAM setup, pick solid_tool.

Create a tool: type = solid_tool, subtype = probe.

Export Tool to Library.

Mark Rief
Retired Siemens

Re: probe dia output / tracking

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Mark,

 

thanks for the info.  i was able to create my own probe.  ( i cant search inside nx help due to a java update and IT aproval)  so thank you for the step by step.  after all of that, i still cant get the tracking points to work.  the only work around i have found is to enter half the probe tip dia into the stock box.  after that, it will probe to actual diminsion i was looking for.  any other ideas?

 

the probe dia is 6mm (.2362 ).  so half of 6mm = .1182

 

adding -.1182 into the stock field

 

T01 M06 (HAAS_PROBE_6MM_BALL)

G65 P9810 X0.0 Y6.25 Z3. F400.

G65 P9810 X0.0 Y6.25 Z1.3819 F400.

P9811 Y6. S54 **************Y6.00 value is corect

G65 P9810 X0.0 Y6.25 Z3. F400.

 

without adding -.1182 into the stock field

 

T01 M06 (HAAS_PROBE_6MM_BALL)

G65 P9810 X0.0 Y6.3681 Z3. F400.

G65 P9810 X0.0 Y6.3681 Z1.3819 F400.

P9811 Y6.1181 S54  this s/b Y6.000

 

 

Re: probe dia output / tracking

What is this variable set to in your post?

 

mom_probing_tool_center_output

 

Jake Hardwick
CNC Programmer
Senior Aerospace AMT
Production NX8.5.3.3 Beta testing NX10.0.1.4

Re: probe dia output / tracking

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Great question.  i just looed in all of the custome commands that were labled probe and did not find this variable.  is there a specific location i would find it or write it?

Re: probe dia output / tracking

I found it using Ken's MOOG_Show_Globals procedure.  Do you have this downloaded and loaded in your post?  If not I would HIGHLY recommend it! It is very useful to get all the variables that aren't listed in the variable browser in PB.

 

Here's the post with the code

Jake Hardwick
CNC Programmer
Senior Aerospace AMT
Production NX8.5.3.3 Beta testing NX10.0.1.4

Learn online





Solution Information