Cancel
Showing results for 
Search instead for 
Did you mean: 

right angel head nc code output

Experimenter
Experimenter

 Hi,

 

I have  integrex-i200 machine and also a post-processor for that. I just want to ask if I will use right-angel head, do I need to edit anything inside the post-procesoor? Or it will works properly since it is working in 5-axis machining?

 

Thank you.

 

 

1 REPLY 1

Re: right angel head nc code output

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think the basic motion will be fine without editing the post.

There may be some issues with (e.g.) G43.4, if you don't also correctly define the tool on the machine.

You would have to test.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information