Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

rough bore ID operation misbehaving

Pioneer
Pioneer

hello,

 

i'm trying to create a rough bore ID operation but for some reason it isn't processing all of the blank geometry, any idea how can i fix this? a picture and the files concerned will be attached below

 

Thanks

2 REPLIES 2

Re: rough bore ID operation misbehaving

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Hi,
try to unset axial trim plane 1 - and you see the result.
and if it is needed, use another combination of trim option (for example radial instead axial 1 )
Vavrusa Ondrej
NX10.0.3
NX11.0.x testing

Re: rough bore ID operation misbehaving

Pioneer
Pioneer
Thank you so much it is now working perfectly, and i'll make sure to do that from now on

Learn online





Solution Information