Cancel
Showing results for 
Search instead for 
Did you mean: 

save problem

Pioneer
Pioneer

I get save failed message with NX10.0.3.5. It is really annoying once you are working on a part in Manufacturing and forget to save for about 30 minutes. All the work is lost. I have experienced this problem in the past and the solution was to Save As another part file. Now, this is not helping as well.

System log is saying following:

 

>>>> Severe error 69 caught in file "D:\workdir\Patches\nx1003_patch\src\part\no\ind\part_save.c" at line number 5486
+++ No saved stack from last exception: thread 9600
*** EXCEPTION: Severe error 69 in line 236 of o:\ugnx1003\ip5\src\syss\no\ind\Error_Severe.cxx at Wed Apr 12 08:40:37 2017 Central European Daylight Time
+++ C++ std::exception caught: Unknown exceptio

 

I am not sure why it is referencing to D drive once NX is installed on C drive.

 

thanks in advance

2 REPLIES 2

Re: save problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe the "D:\" is where the developer had the source file when it was compiled/linked.

 

If you have the whole syslog, I would send it to GTAC for debugging, but at this point it is probably going to be hard to figure out what went wrong.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: save problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

PS...

Are you running any Maintenence Packs ("MPn")?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information