Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

set FMAX in NX CAM

Valued Contributor
Valued Contributor

 can i set FMAX (F15000) in NX CAM

2 REPLIES 2

Re: set FMAX in NX CAM

Siemens Phenom Siemens Phenom
Siemens Phenom

You can do this under Feeds and Speeds, expand Rapid, change motion to G1, enter feedrate. I would creat a custom template and set in all the operations as to not do it every time.

ScreenHunter 34.png

Re: set FMAX in NX CAM

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or are you asking is there a way to limit the posted output to 15000?

In which case (in post Builder, I would assume that Post Configurator can do this as well):

"Program & Tool Path" tab -> "Program" tab -> "Machine Control" (in list on left)

Scroll the right side down & click on the "Feedrates" option

Here you can control max & min feedrates for all feedrate modes (as well as most other feedrate specific settings)

 

If not that, you will have to clarify your question.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information