Cancel
Showing results for 
Search instead for 
Did you mean: 

simulating G-code without workpiece

Creator
Creator

hi,
I am a beginner in NX CAM. I want to simulate the movement of a G-code created in another software. It only contains the x,y,z- coordinates. I just need a simulation of the toolpath movement without the workpiece.
Is this possible ?
please send me feedback
Yannick

1 REPLY
Highlighted

Re: simulating G-code without workpiece

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes this is possible. Prerequisite is that the NC Controller is supported by the existing ones shipped with NX, if not customization comes into play. You need to have a CAM part file including the tools you are using, but it is not needed to have the workpiece. As soon as you like to see material removal you need to define a blank work pieces e.g. a tube or cube.

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information