Cancel
Showing results for 
Search instead for 
Did you mean: 

tool vector calculation

Pioneer
Pioneer

Hello,

Can someone know how to calculate the tool vector angle?

For instant:

CL File: GOTO 12.3, 50.2, 30.5 0, -0.5625358,0.99525365

NC File: G0 X12.3 Y50.2 Z30.5 A??   C??

 

Thanks!

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
8 REPLIES 8

Re: tool vector calculation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You no need to calc this angles manually (of course, you can do it if you want, but - no need). Open PostBuilder and create new postprocessor for your cnc machine. Define type of machine - table-table, table-head, head-head. Set axis for each table-head - C around Z, A around X etc. Save postprocessor and prostprocess any path. You will see needed angles. Thats all.

 

Another way - trigonometryc formulas, paper and pencil.

Re: tool vector calculation

Pioneer
Pioneer
Would I like to know trigonometric formulas for this?
-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!

Re: tool vector calculation

Gears Phenom Gears Phenom
Gears Phenom

That would be good to know.

I suppose there must be machine axis vector and tool axis vector in that calculation.

And after calculating some matrix - you need to extract angles.

Also calculate  XYZ positions from mcs goto according to rotation matrix.

I am really curious about it too.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: tool vector calculation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Not so difficult.
IJK is tool axis vector.
If K not equal 1.00000 (or < 0.9999999999) calc length = sqrt(i*i + j*j)
Divide i and j to length, normalize ij vector.
For AC table machine C will be arcsin(j/length), use i value to define sign and value for c angle (+- 3.141592...)
A will be arccos(K).

If you can use ugopen c angle will be UF_VEC3_angle_between( Y, ij_vector, Z) and you get C from 0.....360
Y is 0,1,0
Z is 0,0,1

Re: tool vector calculation

Legend
Legend
You can use this calculation only if the axis are orthogonal. If one or more axis are under an angle <> 90 degree, than you need another alogrithm.

Re: tool vector calculation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Of course, my formulas for classic AC table. But for any 5 axis cnc this calculations not so complex, more easy vis inverse kinematic task for robots..

Re: tool vector calculation

The postprocessor should output these angles. The calculations based onthe kinematics of the machine are part of NX. 

Mark Rief
Retired Siemens

Re: tool vector calculation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Absolutely agree and my first answer a same.

Learn online





Solution Information