05-23-2016 07:02 PM
05-24-2016 09:07 AM
Hi Claudio,
You can create this kind of tool using the template mill_multi_axis > MILL_10_PARAMETER tool.
Now, you need define the right values for the tool you want.
Below I'm sending an example.
05-24-2016 09:09 AM
05-24-2016 12:25 PM
I have also used a barell cutter for this tool. I had to reduce the neck diameter slightly.
With either 10-param or barrel, I think it is easiest if you use a sketch where you can input the catalog values as expressions, and extract the parameters you need for the tool.