Cancel
Showing results for 
Search instead for 
Did you mean: 

toolpath a raster image

Experimenter
Experimenter

Is it possible to have a toolpath run on an image the has been rastered onto a surface?

6 REPLIES

Re: toolpath a raster image

Pioneer
Pioneer

Good question.  I'd like to know myself.   Have you used Art in Mastercam?   

 

 

Re: toolpath a raster image

Experimenter
Experimenter

I'm not sure, open Jpg image, vectorize it and create the Engraving toolpath.

photo editor

Re: toolpath a raster image

Experimenter
Experimenter

Yes I have. I don't see the need to raster an image if it can't be toolpathed.

Re: toolpath a raster image

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you mean anything like PNG, JPG, TIF, etc., then no, there is no function to machine such things.

If you mean something else, you will have to describe in more details.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: toolpath a raster image

Phenom
Phenom

There are programs that will "Emboss" an image

Some create toolpaths directly.

Others create 3D geometry usually faceted (STL)

 

I have used Blender to create embossed images, the input image needs to be formatted such that colour/grey shade maps to a height.

 

Re: toolpath a raster image

Experimenter
Experimenter

Watch this video.

 

https://vimeo.com/83654051

Learn online





Solution Information