Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

trigger for G99 G98 with hole making

Pioneer
Pioneer

what triggers G99 G98 when using hole making?  With the Drill operations you set the Rtrcto to manual or auto.  But I can't seem to find a setting in the hole making stuff.

2 REPLIES 2

Re: trigger for G99 G98 with hole making

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

hello,

 

in drill, old drill operation - you can set it in cycle setting -rtrct to - auto, manual, etc.

and it outputs G98/99.

But in case of G99 (manual) tools stay in clearence plane - you have to output Z retract motion.

 

In holemaking it is automatic.

When you set transition/rapid - non cutting moves - direct between features - G99

if you set it to clearence plane - G98

 

It works for me this way.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: trigger for G99 G98 with hole making

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Non-Cutting moves - Transfer/Rapid - Between Features  Direct or Clearancenon-cut.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information