Cancel
Showing results for 
Search instead for 
Did you mean: 

trigger for G99 G98 with hole making

Pioneer
Pioneer

what triggers G99 G98 when using hole making?  With the Drill operations you set the Rtrcto to manual or auto.  But I can't seem to find a setting in the hole making stuff.

2 REPLIES 2

Re: trigger for G99 G98 with hole making

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

hello,

 

in drill, old drill operation - you can set it in cycle setting -rtrct to - auto, manual, etc.

and it outputs G98/99.

But in case of G99 (manual) tools stay in clearence plane - you have to output Z retract motion.

 

In holemaking it is automatic.

When you set transition/rapid - non cutting moves - direct between features - G99

if you set it to clearence plane - G98

 

It works for me this way.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: trigger for G99 G98 with hole making

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Non-Cutting moves - Transfer/Rapid - Between Features  Direct or Clearancenon-cut.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information