Cancel
Showing results for 
Search instead for 
Did you mean: 

turning tool in a right position in millturn simulation

Pioneer
Pioneer

Hello,guys
Currently i want to make simulation in NX millturn. But i do not know how to make turning tool in a right position. please see image as blow!
Thanks!Millturn.JPG

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
1 REPLY 1

Re: turning tool in a right position in millturn simulation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Briefly...

In the machine definition, you need to make sure the pockets/tool mount junctions correctly

In each tool, you need to make sure the mount junction is correct

 

I would suggest (if the lower turret can NOT use same toolholders as the upper turret) that you define different holding systems for each so you can't load an upper turret tool into the lower turret, or vice-versa.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information