Cancel
Showing results for 
Search instead for 
Did you mean: 

turning trying to omit reversal on one location

Valued Contributor
Valued Contributor

for one location in this part i would like to omit reversals. the path looks okay in the other sections. has anyone had this problem and what have they done to correct it. it is the area with the arrow pointing to it. I tried to offest the lower line in the groove, but the line next to it is angled and it didn't too well. thanks

 

outerring.JPG

Using NX 8.0.3.4
1 REPLY

Re: turning trying to omit reversal on one location

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sometimes (depends on geometry) this can be done in cut region containment (I typically use points, not planes).

 

If it can't be done with containment, try "Custom part boundary data" -> ingore members

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information