Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

update post from tool preference

Creator
Creator

I am trying to use "mom_tool_adjust_register" in shop doc.

But i get no value in the output documentation.

If i check the template this is what i see.

"Value of the tool length adjust register.  Used only if update post from tool preference is set to on.".

So my question how to do i change preference to update post from tool.

 

Thanks

 

4 REPLIES 4

Re: update post from tool preference

Do you see the variable set in the review tool?

This is the best way to see what is available, and when, in shopdocs.

Mark Rief
Retired Siemens

Re: update post from tool preference

Pioneer
Pioneer

anyone find the answerto this?  Where do you set this preference?

 

I have a tool path that when posted from my pc I get the H word but when posted from   adifferent pc I don'tgetthe H.  Same NX file, same post.  Must be a setting somewhere.  Anyone know aboutthis?  thnks

Re: update post from tool preference

The preference for “Update post from tool” was removed in 2003 in NX2.

I would look at the CLSF output preference “Force LOAD and TURRET”.

Mark Rief
Retired Siemens

Re: update post from tool preference

Pioneer
Pioneer

this ifxed it.

 

file >utilits>user defaults>manufaturing>output>clsf>  check "force LOAD and Turret"

 

 

don't ask me why, but it works.

Learn online





Solution Information