Cancel
Showing results for 
Search instead for 
Did you mean: 

what is the best method for a slot machine on a taper surface

Pioneer
Pioneer

What is the best method for a slot machine on a taper surface. A sample part is attached.

Please suggest a best / optimum method for machining. In existing method of machining problem lies in abrupt Z movement at 2 ends of the slot. Somehow tool path is not smooth.taper_mac.jpg

13 REPLIES 13

Re: what is the best method for a slot machine on a taper surface

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Planar mill with engage set to "Ramp on shape" is one option (may depend on floor geometry of pocket)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: what is the best method for a slot machine on a taper surface

Pioneer
Pioneer

its a thru pocket on a taper and semi arc type surface. please refer the attached file.

 

 

thanks

Re: what is the best method for a slot machine on a taper surface

Legend
Legend

In your Solid Profile 3D operation, set as follow:

 

1. Cutting Parameters > Stock > Tolerance >

     Intol = 0.1mm

     Outtol = 0.1mm

 

2. Cutting Parameters > Corner> Smoothing >

      Z-Axis Smoothing = ON

      And set ramp angle to 30deg

 

3. Turn on whatever compressor that comes with your controller and you are done Smiley Wink

Re: what is the best method for a slot machine on a taper surface

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi, Rudra!

For this case for me more easy to use old-good Sequential Milling operation. I buil sample, just sample, you can change engage, increment for passes, feeds etc.

 

Re: what is the best method for a slot machine on a taper surface

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi, Rudra!

For this case for me more easy to use old-good Sequential Milling operation. I buil sample, just sample, you can change engage, increment for passes, feeds etc.

 

 RUDRA.png

 

 

Re: what is the best method for a slot machine on a taper surface

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

How about using CONTOUR_PROFILE as a more modern way to get a tool path like with sequential milling?

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: what is the best method for a slot machine on a taper surface

Pioneer
Pioneer
Can I get the procedural video of this milling technique?

Re: what is the best method for a slot machine on a taper surface

Pioneer
Pioneer
Is it the only solution?
Highlighted

Re: what is the best method for a slot machine on a taper surface

Legend
Legend

One have fixed your tool path, another have used elementary NX features, and another suggested you to use Contour Profile (which you should have done so from the start).

 

And you are asking for a solution? wt...

 

There are about 20 something different ways to cut that slot with NX. And there are about a million other ways to find out how if you are really interested in finding a solution to your problem.

 

G2/G3 with a Z motion. You can gcode this in notepad in < minute. Geez man...

 

Learn online





Solution Information