Cancel
Showing results for 
Search instead for 
Did you mean: 

zlevel 5 axis

Innovator
Innovator

I'm looking for a bit more tool axis control in NX 8.5 ZLEVEL_5AXIS milling.  I checked the options for customizing the dialog but nothing comes up.  I want to set the maximum step and/or maximum tool axis change per step.  Is there a dialog template that I should look for?

 

Thanks

George

 

George R. Bennett
GRB Consulting
W7 Ult
Various NX versions from 6 to 9
Dell Precision M6700
3 REPLIES 3

Re: zlevel 5 axis

George,

Try generating a 3 axis zlevel path, and then using Tilt Tool Axis in the Operation Navigator.

This provides control for the max tool axis change in degrees per step and max step.

Mark Rief
Retired Siemens

Re: zlevel 5 axis

Innovator
Innovator

I see the option Mark but I get a license server error when I select it.  I have a MACH 3 license.  Which bundle do I need to access it?

 

Thanks

George

 

George R. Bennett
GRB Consulting
W7 Ult
Various NX versions from 6 to 9
Dell Precision M6700
Highlighted

Re: zlevel 5 axis

George,

The bundles are adjusted periodically, so I don't know exactly what you have.

 

In today's bundles, it is included in "NX Advanced 5 Axis Machining [NX13440]"

 

In your license file, the feature is "nx_tilt_tool_axis"

Mark Rief
Retired Siemens

Learn online





Solution Information