Cancel
Showing results for 
Search instead for 
Did you mean: 

Active Pictures Plug-ins for Simcenter available

Community Manager Community Manager
Community Manager
Comments
Enthusiast
Enthusiast

LMS Test.Lab 17 link link does not work.

Dreamer
Dreamer

The link for Test.Lab17 not working

Siemens Phenom Siemens Phenom
Siemens Phenom

The rev 17 link is now working.  

Siemens Visionary Siemens Visionary
Siemens Visionary

The broken link to LMS Test.Lab 17 Active Pictures plug-in is now restored!

Dreamer
Dreamer

LMS Test.Lab 17 does not seem to work. Download gets interrupted about halfway.

Dreamer
Dreamer

the link for 17.1 seems doesn't work for me, get interrupted in halfway. 

 

Dreamer
Dreamer

Hi 

 

Great to be able to access these - thanks! 

 

Unfort., I have an installation problem (tried both 14A and 15A). I get an error at the final step (possibly something to do with Firewall since this is the last message the Installer gives). 

 

LMS TL Active Pictures installation problem 11-07-18.PNG

 

Anyone got any ideas, please? I'm installing on the following system:

 

FEIT015835.JPG

 

Many thanks, Ben (Benjamin.Halkon@uts.edu.au)

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Ben,

 

If you right click on the executable and select Run As Adminstator it should work.  I think the installation is having trouble writing some information to the registry or writing into the installation directory.  Note the active picture \ data plugin is only for non Test.Lab computers since this functionality is installed with Test.Lab.  If this does not resolve your issue, please reach out to your local Global Technical Assistance Center (GTAC) and they can assist.

 

Kevin