Cancel
Showing results for 
Search instead for 
Did you mean: 

High Quality Movie Capturing

Siemens Phenom Siemens Phenom
Siemens Phenom

  

  • Capture movies in any resolution, framerate and duration needed
  • Adjustable compression in .mp4/h.264-format
  • Synchronized with the simulation-time, or if needed slower or faster
  • Produce movies in side-by-side-stereo for playback on stereo capable devices

Example:

(view in My Videos)

 

Introducing cameras, camera-views and camera-motion during simulation:

cam.jpg

 

Fast and easy modelling of camera pathes, by saving the current view:

(view in My Videos)

 

Download the right package for your platform and enjoy!

Comments
Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

I successfully installed the add-on, but when i try to create engineering library for the Moviecamera_Robot.cojt camera model, an error message appears:

"The file is not valid for the following reason: Syntax error in line 26."

What could be the cause of this?

 

Siemens Visionary Siemens Visionary
Siemens Visionary

Can you please check that tunedata.xml in the cojt is valid? You can delete it and create new one if you are not sure.

 

Pioneer
Pioneer

Hello,

 

is it exists package also for PS12.1, please?

 

Thank you

Genius
Genius

HI

I am also interested in knowing if anything will be avaliable for Tx12.1

Tried the package for 11.1 but it does not work..

It was such a nice tool!!!

 

/Andreas

Valued Contributor
Valued Contributor

Hi!

 

Has as a create a DLL for 11.1TR3 version?

 

Because when I go register the DLL generates this error below:

 

2016-08-18_08-36-02.png