Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Smart Reporting tools with MotorSolve

Siemens Visionary Siemens Visionary
Siemens Visionary

The information below was gathered from the 2018 Simcenter Conference - Americas that took place October 15-17 in Detroit, Michigan.

 

detroit event collateral.jpg

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Author: Steven Huard - Parker Hannifin Corporation 

 

Customizing the reporting mechanism in MotorSolve can have a substantial impact on your productivity. Significant time is saved by configuring several batch motor experiments to analyze ahead of time, hence allowing the various simulation to run in the back ground while the user is working on other things. The application delivers the simulation inputs to MotorSolve, runs the simulation, places the results into the report and then starts over again with the next simulation and repeats until all the simulation are done.

 

This is all done without user interaction, other than filling in a form and starting the process.  When all of the simulations are complete, the results are assembled into a single MotorSolve report containing the various MotorSolve results.