Cancel
Showing results for 
Search instead for 
Did you mean: 

TLG Aerospace: Successful Applications of CFD within the Aircraft Certification Process

Community Manager Community Manager
Community Manager
rencen.jpg

The information below was gathered from the 2018 Simcenter Conference - Americas that took place October 15-17 in Detroit, Michigan.

 

Author: Andrew McComas, Engineering Manager

 

Aircraft manufacturers who seek certification are required to demonstrate compliance airworthiness regulations. Since flight test to the corners of the envelope is not practical or safe, development of a high fidelity full-vehicle virtual-model is critical to the successful completion of any certification program. For airplanes where structural flexibility is important, these models require a coupled aerodynamic and structural solution. Advances in CFD robustness, accuracy and simulation run-times have made it a viable replacement tor wind tunnel testing. This approach is often referred to as Certification by Analysis. Learn how TLG Aerospace utilizes Simcenter STAR-CCM+ to generate the aerodynamic database that informs the aero-structural models used for loads, flutter, and handling qualities.