Cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual Waterproof Testing

Siemens Visionary Siemens Visionary
Siemens Visionary

The information below was gathered from the 2018 Simcenter Conference - Americas that took place October 15-17 in Detroit, Michigan.

 

detroit event collateral.jpg

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Author: Vineet Rakesh and Mark Goodrich

 

Waterproof testing is performed to determine water ingress and membrane failure due to spray impingement. This presentation will explain how STAR-CCM+ can provide a combination of multiphase modeling techniques which enabled virtual waterproof testing.

These models provide detailed quantitative information unavailable through experiments such as reduction in prototyping time and costs, and better understanding of the mechanisms involved. In addition, powerful VOF-LMP coupling will be available in upcoming Star-CCM + releases and would allow detailed characterization of nozzle flow. Transitioning to STAR-CCM+ has helped our team accelerate the model development and design iteration phases.