Showing results for 
Search instead for 
Did you mean: 

export laser projection


When exporting laser projection files for assy guidance with parts that have multiple laminates. Do the laminates have to be linked as parent and child to create a single laser program? It seems if not I have to create a separate program for each laminate. Is there a way to turn this off?


Re: export laser projection

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Laser projection will allow selection of all children of the selected laminate.  The most common way to export plies with mulitple laminates is to have them linked (e.g. in a core panel the overcore laminate would be linked to the OML laminate).  This is also beneficial in other areas such as 3D Cross Sections.  Another option is to have a top-level collector laminate and parent all other laminates to it.  You can think of the collector laminate as the assembly and the child laminates as the parts.

Re: export laser projection


Hi Crazyhorse,

One other thing to be careful of if creating separate laser projection files for each laminate, is whether or not your laminates use separate surfaces that represent the underlying structure (e.g. undercore and overcore surfaces) or share a common lay-up surface.  The former case is usually fine, but the latter may cause some issues.

We sometimes use multiple laminates on a single layup surface to simplify the design process - e.g. they may represent different material groupings, or be used to model complex changes in ply drop-off geometry that can be difficult to handle within a single laminate.  In this situation, if laser files are generated for each stand-alone laminate, Fibersim (at least the version we use), will treat each projection as starting from the original layup surface and will not take any underlying plies into account. 

For this type of design, linking them through a parent-child relationship, or under a collector laminate (with appropriate sequence-step values), proved to be the only way to generate accurate laser projections.



Re: export laser projection

That's a good point. I have couple parts that I should probably review.
Thank you.

Dan Hoelter
NC programming
Work 314-264-3621
GKN Aerospace
142 McDonnell Blvd.
Hazelwood, Mo. 63042

"This e-mail is confidential and contains information proprietary to GKN that may be covered by legal, professional or other privilege.Recipient may use such information only in the context of the terms of the existing agreements in effect between both parties. The sender does not give any warranty as to the completeness of this e-mail. If you are not the attended addressee you may not use, disclose or copy this transmission."

WARNING: This document may contain technical data whose export is restricted by the Arms Export Control Act (Title 22, U.S.C., SEQ 2751 ET SEQ) or the Export Administration Act (Title 50, U.S.C., APP 2401-2420). Violations of these export laws are subject to severe criminal penalties.
This e-mail is strictly confidential and intended solely for the addressee. It may contain information which is covered by legal, professional, or other privilege. If you are not the intended addressee you must not use, disclose, or copy this transmission. This E-mail is not intended to impose nor shall it be construed as imposing any legally binding obligation upon any of the GKN group of companies ("GKN"), and/or any subsidiaries thereof or associated companies thereof. Neither GKN nor any subsidiaries thereof or associated companies thereof gives any representation or warranty as to the accuracy or completeness of the contents of this E-mail. GKN shall not be held liable to any person resulting from the use of any information contained in this E-mail and shall not be liable to any person who acts or omits to do anything in reliance upon it. Unendorsed export or re-export is prohibited.