Cancel
Showing results for 
Search instead for 
Did you mean: 

Optimizing NX display settings for use with Fibersim

Community Manager Community Manager
Community Manager

As Fibersim relies on linking to CAD curves, then displaying boundaries overlayed upon them, the quality of the display is critical to a clear understanding of what is being highlighted.  In NX, this “display geometry” uses the user-defined part and session settings for curve display.  Changes in NX 10 drafting resulted in some default line settings that have a negative impact on the visibility of Fibersim’s display geometry.  Following are a few simple tips for ensuring that your NX settings are optimized for displaying Fibersim geometry:

  1. Show Widths
    • Make sure you have the “Show Widths” option turned on. This can be found under File > Preferences > Visualization > Line.
  2. Reset Pixel Widths
    • Once the Show Widths option is turned on, the “Pixel Widths” will be used to assign a set number of pixels to each of the 9 widths. Fibersim is set up to display geometry using the 1st, 3rd, and 4th widths, and assumes that they are each set to 1, 3 and 4 respectively as that was the default when the 9-width format was introduced in NX 9.
    • With NX 10, the default value of the first 4 widths was assigned as 1 pixel, meaning that all Fibersim geometry will display as “thin” lines. To optimize this, assign each width an ascending thickness from 1-9 as follows:NXDisplaySettingsPixelWidths.jpg
    • As these settings are stored with the part, each part must be reconfigured separately.
    • Tip: If you configure your Customer Defaults (File > Utilities > Customer Defaults > Gateway > Visualization > Line) with these width values, you can simply press “Reset to Defaults” and NX will copy in your default values into the work part.
  3. Make CAD curves thin
    • Depending on your default object settings, step 2 may make all your existing curves and edges very thick (the default NX 10 setting is .70mm, which will go from 2 to 6 pixels!)
    • To change existing curves and edges, simply select all (CTRL+A) without any selection filter, Edit Display settings (CTRL+J) and set the object Width to the thinnest setting:
    • EditObjectDisplay.jpg
    • To make the change for all future curves and edges, change the Object Preferences (File > Preferences > Object ) setting for Width to the thinnest setting
    • Tip: to ensure future parts respect the same thin width settings, you can make the same change to your Customer Defaults (File > Utilities > Customer Defaults > Gateway > Object > Default > Width)
  4. Disable Wireframe Contrast
      • The final optimization affects the color of the Fibersim display geometry. Most Fibersim display geometry is colored green, blue, red or yellow, depending on the orientation of plies.  NX has a visualization setting designed to improve the contrast of wireframe geometry when viewed against a light background that alters these colors and makes them all a bit darker and drabber.
      • To disable this setting and restore the true colors, go back to the line visualization settings (File > Utilities > Customer Defaults > Gateway > Visualization > Line) and uncheck “Wireframe Contrast”
      • Since this is a session setting, it only needs to be changed once, after which all parts will be displayed in the same manner.

     

     

     

    BeforeBefore 

 

 

 

 

 

 

 

 

 

 

 

 

 

AfterAfter