Cancel
Showing results for 
Search instead for 
Did you mean: 

Adding a new MindConnect Element and configuration of MindConnect Data Models

Community Manager Community Manager
Community Manager

How can I add a new MindConnect Element and start the configuration? 

27 REPLIES

Betreff: What MindConnect elements are available to connect to MindSphere?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi @vnsuper,

 

You can connect a new MindConnect Nano with the "IoT Data Modeler". After opening the App you can add a new Asset and then you have to choose the MC-Nano. After this you can configure your MC-Nano.

Re: What MindConnect elements are available to connect to MindSphere?

Pioneer
Pioneer

Hi Steffen1,

 

It seems works I can see the steps to configure as in the document. Thanks for let me know that.

Re: What MindConnect elements are available to connect to MindSphere?

Pioneer
Pioneer

Hi Steffen1, 

 

I setup the MindConnect Nano device. After plug USB with configuration information exported from IoT Data Modeler into device. After a while, the device has two lighting leds:  RUN/STOP/L1 orange,  PC ON/WD is green. I check in asset in the web, I see Onboarded column is green but Online column is still gray. I also see the log file (generated in USB) I see some lines.

 

2017-12-08 03:00:36.429 Loading module DiagnosticLogger:
2017-12-08 03:00:36.429 Connection to Mindsphere could not be established. Please check the network configuration or local network environment. (Error 12)

 

Is my device connected properly? Thanks.

Betreff: What MindConnect elements are available to connect to MindSphere?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Good morning, @vnsuper,

 

Do you have more informations?

 

Have you collected the Logs from your MC-Nano with the "ConBox_Commands.json" File?

 

After collecting the Logs we can take a deeper look whats going wrong.

Re: What MindConnect elements are available to connect to MindSphere?

Pioneer
Pioneer

Hi Steffen1, 

 I just see 2 log file generated in USB. The 1st I just shown, the 2nd file content is something like below. Note that I plug/replug USB several times. Thanks.

 

Fri Dec 8 03:00:32 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's USB_STICK state was changed to ACTION_IN_PROGRESS
Fri Dec 8 03:00:32 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's USB_STICK state was changed to USB_INACTIVE
Fri Dec 8 03:00:33 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's CONNECTION state was changed to CONNECTED_TO_CLOUD
Fri Dec 8 03:00:33 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to NOT_ONBOARDED
Fri Dec 8 03:00:36 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to ONBOARDING_IN_PROGRESS
Fri Dec 8 03:00:37 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to ONBOARDED
Fri Dec 8 03:00:40 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to ONBOARDED_LOCKED
Fri Dec 8 03:02:00 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's USB_STICK state was changed to ACTION_IN_PROGRESS
Fri Dec 8 03:02:01 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's USB_STICK state was changed to USB_INACTIVE
Fri Dec 8 03:02:01 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's CONNECTION state was changed to CONNECTED_TO_CLOUD
Fri Dec 8 03:02:01 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to NOT_ONBOARDED
Fri Dec 8 03:02:04 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to ONBOARDING_IN_PROGRESS
Fri Dec 8 03:02:06 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to ONBOARDED
Fri Dec 8 03:02:09 2017 (SAL V01.01.00.02 b005|CONBOX V04.00.20.17 b066) Agent's ONBOARDING state was changed to ONBOARDED_LOCKED

Re: What MindConnect elements are available to connect to MindSphere?

Pioneer
Pioneer

Hi Steffen1, 

 

I'm also setting another MindConnect IoT2040. But I encounter a problem so I would like to add question here too. When I power up the device, I see 3 lighting LED s

+ PWD: green

+ USB: green

+ USER: red (no blinking)

 

According to document that mean there's a problem with firmware in device. However, I just use this device for the first time, I have yet update any thing on the device yet. Please help me a solution for fixing the device issue. 

 

Thanks in advance.

Betreff: What MindConnect elements are available to connect to MindSphere?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi @vnsuper,

 

you can update your MindConnect IoT2040 with the newest Firmware. When the Firmeware is to old, the Device isn't able to update the Firmeware automatically, so you have to do it per USB-Stick.

 

You can download it here in the SIOS: MindConnect_IoT2040_FW

 

1. Download the fw.zip file

2. Extract files

3. Copy the fw.tar file to an empty USB-Stick

4. But the USB-Stick to the MindConnect IoT2040

5. Wait a few minutes. The device will reboot a few times.

6. Check the Logfiles on the USB-Stick. In one of the Files you will see, that the firemware was updatet or that something went wrong.

7. After successfully updating the Firmeware your device will be ready for the onboarding process.

8. Make the Configuration in the IoT Data Modeler and try to onboard your MindConnect IoT2040

 

Let me know if that works.

 

See you,

Steffen1

Re: What MindConnect elements are available to connect to MindSphere?

Pioneer
Pioneer

Hi Steffen1. Thanks for your information. I'll try with the device next week when I come to office.

Re: What MindConnect elements are available to connect to MindSphere?

Pioneer
Pioneer

H Steffen1

 

I follow your direction, when I plug USB into IoT2040, it restart after 30s. After waiting for 15 mins, I notice 3 lighting LED is still the same as before.

 

I decide to go ahead with reload configuration exported from Cloud. When I plug USB with data model configuration, I see the device can restart automatically now. After waiting for 15 min, however, the device is still not onboarded in Mindsphere cloud. The lighting leds are the same behavior as before.

Please help to check.