Cancel
Showing results for 
Search instead for 
Did you mean: 

I cannot edit the general settings of an asset

Experimenter
Experimenter

Hello,

 

I want to edit the general settings of an asset, but everytime i want to do this, error 500 occours. Because of this i can´t use Map View in the Fleet Manager. Can anybody tell me what´s the reason of this problem?

2019-02-11 14_46_17-Asset Manager.png

1 REPLY 1

Re: I cannot edit the general settings of an asset

Valued Contributor
Valued Contributor

@pkram can you try again? For me it worked in Asset Manager.

Other hint: You could also move the position of assets in the Fleet Manager directly via the edit functionality:

- Start the edit mode.

- Single assets can directly be moved by drag and drop.

- In clustered assets you have to select one and then can also move it by drag and drop.

- Confirm the changes to get them active.