Cancel
Showing results for 
Search instead for 
Did you mean: 

MindConnect FB 1500 proxy

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi all,

I want to upload data from PLC S7-1500 to MindSphere using MindConnect FB 1500. When the PLC tries to onboard, the process failed with error 16#8001 Communication error. I think the problem is that the PLC is connected to the Internet through corporate proxy. Is there a way to configure proxy connection in the PLC or relevant DBs?

Thanks.

1 REPLY 1

Betreff: MindConnect FB 1500 proxy

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi @lad,

 

I'm sorry put the MindConnect-FBs doesn't  Support Proxy. The reason for this is, that the PLC does not support proxy. For more informations see technical details of the PLC.

 

See you,

Steffen1