Cancel
Showing results for 
Search instead for 
Did you mean: 

POST not available in self-MindApp

Siemens Creator Siemens Creator
Siemens Creator

Hello,

         After pushed application. the app has two url:

         1)appName.appsdev.mindsphere.io, in this link, the post interaction is OK

         2)After register, the app link: tenantaccount.appsdev.mindsphere.io/apps/appname. but in this link, the 

POST API returns 403 forbbiden.

          Pls help me confrim the problem, thank you very much.

4 REPLIES

Re: POST not available in self-MindApp

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
Hello,
have you solved your problem?
I have the same error and want to know if you have a solution for this.
Thank you.

Re: POST not available in self-MindApp

Community Manager Community Manager
Community Manager

Can both of you confirm that you have a Developer Package size M or L? Its not possible to publish applications to productive with a S.

 

Tabelle

Re: POST not available in self-MindApp

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
i have a Develper Package M and my app is running on the development system.
I just want to call a Post method to send some data to the app user, but when I send the post, I get the errorcode 403.

Re: POST not available in self-MindApp

Community Manager Community Manager
Community Manager
Errorcode 403 is the referring to an authentication issue and that the user is authenticated but isn’t authorized to perform the requested operation on the given resource. In this case, it might be that something is twisted with your access right, I therefore recommend you to get in touch with our development support since they can take a deeper look.

You can get in touch with them via the Siemens Industry Support here: https://support.industry.siemens.com/My/ww/en/requests#createRequest