Cancel
Showing results for 
Search instead for 
Did you mean: 

Rectangular to round duct transition.

Valued Contributor
Valued Contributor

Is there any way to create a rectangular to round duct transition in 180 degree segments and bend lines so this can be fabricated in sheet metal? And if there is not when will this happen?

2 REPLIES

Hi Dave,...did your last transition topic cover this off?...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Dave,...did your last transition topic cover this off?

[ie: ordered mode "lofted flange" using 180 degree sketch profiles, positioned accordingly]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Hi Dave,...did your last transition topic cover this off?...

Valued Contributor
Valued Contributor
Hi Sean,
Thanks for the followup. ordered seems to be the way to go with this particular transition in SE. I lean towards an aftermarket program though that allows me to set up my printer and use standard sheet sizes which it creates a layout and cut template from. Or at the least gives me all the flat co-ordinate points for layout from X-Y zero. Sheet lightning is the one and it is fine for thinner gages. Past say 11gage and I would go with Plate and Sheet as it gives layouts for inner center and outer of flange. SE is not quite there for what i want to do compared to these two programs.