Cancel
Showing results for 
Search instead for 
Did you mean: 

Set up a user only with access to an arrea in V3

Experimenter
Experimenter

I would like give a user access to a specific area under my tenant, ( like in version 2 )

 

is there a whay to do that ?

TSB
2 REPLIES 2

Re: Set up a user only with access to an arrea in V3

Siemens Legend Siemens Legend
Siemens Legend

Hi @Banke, should be coming soon, but not possible yet.  The feature is called the "OEM use case" or "subtenants" so watch out for the announcement about that.  I can try to post here when it is available.

Re: Set up a user only with access to an arrea in V3

Experimenter
Experimenter

OK - thanks

I hope it come soon, because I can't use it before it is implemented ;-(

 

 

TSB