Cancel
Showing results for 
Search instead for 
Did you mean: 

Appearances in PLC Mode with Process Simulate

Creator
Creator

Hi everybody,

 

I have a problem with a simulation created into Process Simulate.

In CEE Mode Simulation the appearances appear but when I switch in PLC Mode Simulation they don't appear.

How can i do?

 

Thanks

2 REPLIES

Betreff: Appearances in PLC Mode with Process Simulate

Gears Phenom Gears Phenom
Gears Phenom

Hi,

with witch function do you create your apperance?

In PLC Mode you must connect all working signals to resource (lb)

only the signals are connected to lb are working.

 

The modul viewer is not available in PLC mode.

Kind regards,

Benjamin Voelzke

Betreff: Appearances in PLC Mode with Process Simulate

Creator
Creator

Hi,

 

I resolved problem. Before I used the Resource Input Signal and appearances didn't appear when I switched in PLC Mode, now I am creating the signals and operations with Create Device Operation/Signals and Create Non Sim Start Signal (Tab Control->Operation Signals) and everything works correctly.

I thought that both CEE  and PLC Mode Simulation could use signals created by Signal Viewer (Resource Input/Output Signal ). This procedure works only in CEE Simulation.

 

Best regards