Cancel
Showing results for 
Search instead for 
Did you mean: 

Auto 2017 & Factorycad 2017: Unhandled Exception e06d7363 (e06d7363h) at address fd6ba06ch

Experimenter
Experimenter

Auto 2017 & Factorycad 2017

 

After installation of Autocad 2017 & Factorycad 2017 + Hotfixes 1,2,3 Factorycad crashes after startig up

 

The Error Code is:

Unhandled Exception e06d7363 (e06d7363h) at address fd6ba06ch

4 REPLIES

Re: Auto 2017 & Factorycad 2017: Unhandled Exception e06d7363 (e06d7363h) at address fd6ba06ch

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Try running cimfcleanregistry17.exe. The default location for this file is in C:\Program Files\Siemens PLM Software\Factory Programs 2017\Program. This will ensure that all of your previous registry entries for the Factory products are removed. After you run this, reload the menus by typing FACTORY in the command window (do not use the CUI command to load the menus). This will make sure all trusted paths are set correctly.

 

If you continue to see this problem, please contact GTAC support at 1-800-955-0000 and they should be able to troubleshoot your install.  

Re: Auto 2017 & Factorycad 2017: Unhandled Exception e06d7363 (e06d7363h) at address fd6ba06ch

Siemens Creator Siemens Creator
Siemens Creator

Hello ,

 

FactoryCAD is based on AutoCAD platform and supports the system configuration requirement of AutoCAD.

Below is the Autodesk link for certified graphics hardware and the supported drivers. Current supported version for most of the NVIDIA Quadro adapters is 385.90. I recommend to download and install from Autodesk link.

 

https://knowledge.autodesk.com/certified-graphics-hardware

 

Another workaround for machines with "not cad graphics card" could be renaming these 2 files.

 

fcad.png

 

As a consequence of this workaround "import jt" command is not working.

 

Please let me know about the result.

 

Best regards

Konrad

Re: Auto 2017 & Factorycad 2017: Unhandled Exception e06d7363 (e06d7363h) at address fd6ba06ch

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

This issue is related to an OpenGL issue. To be able to use the latest NVIDIA drivers you can also try the following workaround:

 

Problem:

The crash is reproduced with drivers that support OpenGL version higher than 4.5

 

Workaround:

Option: Define an environment variable:

Variable: JT_OGL45

Value: 1

Highlighted

Re: Auto 2017 & Factorycad 2017: Unhandled Exception e06d7363 (e06d7363h) at address fd6ba06ch

Experimenter
Experimenter

Kristy,

 

Thank you very much for your workaround recommendation.

We will be trying this workaround first thing in the morning to see if it resolves our issues.

 

If this does resolve our issues I will be accepting this as a solution.


Best regards, 

Ivo Gorissen
System Administrator
VDL Steelweld