Cancel
Showing results for 
Search instead for 
Did you mean: 

Autocad 2009 and Factory Flow release 13.0

Not applicable

Calculation problems when running a flow calculation, some troubles happen; sometime
it's "Autocad Error Aborting : fatal error unhandled e0434f4dh Exception at 7e812afdh"
or when flow recalculates with existing activity points on drawing we get "An unexpected
error occurred while attempting to get activity point names" just after “warning
: 353007 : the SDX name (dock1) is already in use“ after these errors I have to
kill the process to terminate.
What's wrong?
Thank's
1 REPLY 1

Re: Autocad 2009 and Factory Flow release 13.0

Not applicable

"Francois Cossette" wrote:
>
>Calculation problems when running a flow calculation, some troubles happen;
>sometime
>it's "Autocad Error Aborting : fatal error unhandled e0434f4dh Exception at
>7e812afdh"
>or when flow recalculates with existing activity points on drawing we get
>"An unexpected
>error occurred while attempting to get activity point names" just after “warning
>: 353007 : the SDX name (dock1) is already in use“ after these errors I have
>to
>kill the process to terminate.
>
>What's wrong?
>
>Thank's

Hello Francois
We have resolved this issue for the 13.0.1 patch. Please send me an email directly
to deepak.gokuldas@siemens.com and I can send a temporary fix for you until the
13.0.1 patch is available.
Regards
Deepak