Cancel
Showing results for 
Search instead for 
Did you mean: 

Autodesk Inventor data in Process Simulate

Experimenter
Experimenter

Hallo together,

I´ve an very genaral question:

 

I worke with Process Simulate (especially Jack to analyse the human movements, generate ergonomical reports ...).

Now I whant to create a machine from Inventor parts to my Robcadstudy. 

My Problem: I can´t work with the kinematiceditor or create an "New device operation" with this inserted parts.

What I´ve to do to create very simple buildet machines with kinematics from Inventor data?

(It´s a project as a part of my master thesis)

 

Thanks for your help,

Niklas

2 REPLIES
Highlighted

Re: Autodesk Inventor data in Process Simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

I´m not familiar with Inventor but if possible you can export your parts to JT format (monolithic).

 

This JT file you can import into PS.

Afterwards you will have a *.COJT folder including your JT file within your library/systemroot.

 

From this point you are able to open it for modeling (set modeling scope) and afterwards you can run Kinematic Editor.

If you have a *.CO folder will won´t be able to open for modeling.

 

As soon as you have defined any kinematics you are able to create a device operation because from this point your object is a device. Without a kinematics it´s just an object.

 

I hope this helps.

 

Best regards

Patrick

Re: Autodesk Inventor data in Process Simulate

Experimenter
Experimenter

Hi Patrick,

thank you so much! Problem solved!