Cancel
Showing results for 
Search instead for 
Did you mean: 

C# API :Could not load file or assembly DnApplicativeInfra

Experimenter
Experimenter

Hello:
  I'm using version 10.1-64bit,I can not open the TxForm designing which inherited from TxForm in Visual Studio2012. Other configurations and settings are all set up.

360软件小助手截图20141118000203.jpg

 

System Information:

    Microsoft Windows 7
    6.1.7601 Service Pack 1
    System manufacturers: LENOVO
    CPU Intel(R) Core(TM) i7-3740QM CPU @ 2.70GHz
    BIOS 版本/日期 LENOVO G5ET91WW (2.51 ), 2013/1/17

 

Sorry for google english

Thanks

2 REPLIES

Re: C# API :Could not load file or assembly DnApplicativeInfra

Experimenter
Experimenter
Does anyone have a solution for this problem?

Re: C# API :Could not load file or assembly DnApplicativeInfra

Siemens Legend Siemens Legend
Siemens Legend

If I remember correctly, Tecnomatix 10.1 assemblies are built using VS2008 with .NET framework 3.5. Though I believe this should work with VS2012, you still need to make sure that the assembly you are building uses the same .NET framework version.

 

Zachi